<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 5.50.4807.2300" name=GENERATOR><STYLE></STYLE></HEAD><BODY bgColor=#ffffff><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002>Hi Andrew</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002></SPAN></FONT> </DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002>I have seen exactly the same thing as you describe, I just thought that it was one of these "features" in VEE you have to live with.</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002></SPAN></FONT> </DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002>I would be nice to know from Agilent if this is a known bug, and if it is then it would be nice to know if it is corrected in ver. 6.1.</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002></SPAN></FONT> </DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002>Regards</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002>Kenth Jensen</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002></SPAN></FONT> </DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=696385805-16082002></SPAN></FONT> </DIV><DIV class=OutlookMessageHeader dir=ltr align=left><FONT face=Tahoma size=2>-----Original Message-----<BR><B>From:</B> ext Andrew Fudge [mailto:AndrewF@genesysibs.com]<BR><B>Sent:</B> Tuesday, August 13, 2002 1:11 PM<BR><B>To:</B> vrf@lvld.agilent.com<BR><B>Subject:</B> vrf Strange Segmentation violation error #2<BR><BR></FONT></DIV><DIV><FONT face=Arial size=2>Hello All</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>I am sharing my experiences of strange VEE behaviour.</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><FONT face=Arial size=2>I keep getting "Segmentation Violation" errors when opening a certain VEE file for development.</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><FONT face=Arial size=2>I discovered that if I open the file by double clicking, it errors on load and I could not load it.</FONT></DIV><DIV><FONT face=Arial size=2>I launched VEE development and choose File>Open from menu, I open the save file from the same location and it opens fine. This is very strange.</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>When we had a Desktop Shortcut pointing to a VXE file, we would sometimes see the same/similar segmentation error. Then edited the shortcut properties and set the Working Directory ("Start In") to the dir where the file is, and the error seemed to be less persistent.</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>Seems like maybe a similar problem.</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>Any comments/experiences welcomed.</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>Andrew Fudge</FONT></DIV><DIV><FONT face=Arial size=2>Genesys IBS</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2><BR>---<BR>Outgoing mail is certified Virus Free.<BR>Checked by AVG anti-virus system (<A href="http://www.grisoft.com">http://www.grisoft.com</A>).<BR>Version: 6.0.381 / Virus Database: 214 - Release Date: 02/08/02</FONT></DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@it.lists.it.agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
asReal64("0x"+A)
or use a FromString transaction to read in hex format.
Regards,
Bill Ossmann
--
bill_ossmann@hsgmed.com
Philips Ultrasound
>-----Original Message-----
>From: Shaun.Trussler@nokia.com [mailto:Shaun.Trussler@nokia.com]
>Sent: Thursday, August 15, 2002 1:19 PM
>To: VEE vrf
>Subject: [vrf] Converting text (in hex) to a number in decimal
>
>
>
>Greetings All:
>
>I have looked for a function that will take text representing
>a hex number (e.g 2F) that can make a conversion to either
>a INT or Real decimal number (in this case 2F to 47). I
>haven't found a built-in function that will do this and perhaps
>none exists. If so, has anyone written a piece of code that
>will do this? I realize it would be possible to crudely map an
>array of text to an array of decimal numbers but I was looking
>for something more elegant. Thanks for any assistance.
>
>
>
>Regards,
>Shaun Trussler
>
>
>
>
>
>---
>You are currently subscribed to vrf as: bill_ossmann@hsgmed.com
>To unsubscribe send a blank email to
>"leave-vrf@it.lists.it.agilent.com".
>To send messages to this mailing list, email
>"vrf@it.lists.it.agilent.com".
>If you need help with the mailing list send a message to
>"owner-vrf@it.lists.it.agilent.com".
>
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".