AnsweredAssumed Answered

vrf CallableVEE Problem

Question asked by VRFuser on Sep 24, 2002
> You can't do it [call
> VEE from VEE using the
> ActveX client/server].

Wow! That's amazing. I'll let it pass until I can find out exactly why but
until then (if that actually ever happens) all I can say is it's one of the
most amazing things I've ever heard.

[variant arrays]
> I understand it is a
> condition of the ActiveX
> interface.

ActiveX passes one type only: variant. One type of variant is an array of
whatever. Even variant. Thus the specification. It's pretty much the only
way to pass an unknown number of parameters of unknown type. So for input
parameters there's a variant array called Inputs and for output parameters
there's a variant array called Outputs.
-SHAWN-


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes