AnsweredAssumed Answered

vrf Strange things are happening with VEE 5.01

Question asked by VRFuser on Feb 28, 2002
Hi there,

By chance, do you have the "Delete Variables at Pre-Run" check box
cleared in the Default Preferences? This could do what you are seeing.

Mike

-----Original Message-----
From: rpage@futaba.com [mailto:rpage@futaba.com]
Sent: Thursday, February 28, 2002 2:44 PM
To: vrf@lvld.agilent.com
Subject: vrf Strange things are happening with VEE 5.01



A question about program flow and order of operation. I'm reviewing a vee
program from one of our other offices. At one point in the test it checks a
value against a variable. The variable is not set in the main flow of the
program. I would expect that they would be getting a variable not defined
error, but they don't. I found that the variable happens to get defined in a
User Function that never gets called. How is this? I've heard that VEE will
execute any/all functions that has a start button in it simultaneously. Is
this true? Partially true? Unfortunately, I can't step through the program
to see if and when the variable actually gets set.
Has anyone experienced this?
Rick Page
Test/Software Engineer
Futaba Corp of America
1605 Penny Lane
Schaumburg, IL 60187
Tel: (847) 884-1444 x162
Fax:(847) 884-4988
www.futaba.com

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes