AnsweredAssumed Answered

vrf VEE 6.03

Question asked by scubaman on May 29, 2002
Latest reply on May 29, 2002 by scubaman

For the record:  EVERYTHING IS CONSISTENT AND WORKS AS EXPECTED on my win2k
machine.  I don't need to go into where I screwed up, but...  On my win2k
machine, after the update to 6.03

1. whichversion() returns 6.03
2. vee.exe file properties - version shows 6.0.3.0
3. help - about shows 6.03

--
Regards,
Rich
===========================
Richard Kleinhenz
mailto:scubaman@us.ibm.com
845-892-2617
===========================


                                                                                                                               
                      "Pickles, Warren"                                                                                        
                      <picklesw@tycoelect        To:       "'VEE Reflector (E-mail)'" <vrf@lvld.agilent.com>                   
                      ronics.com>                cc:                                                                           
                      Sent by:                   Subject:  RE: vrf VEE 6.1                                                     
                      owner-vrf@lvld.agil                                                                                      
                      ent.com                                                                                                  
                                                                                                                               
                                                                                                                               
                      05/30/2002 03:17 AM                                                                                      
                                                                                                                               
                                                                                                                               



The WhichVersion() function returns the correct version (6.01) on my
system.
I expect that works in 6.03 as well.
Regards,
Warren Pickles




-----Original Message-----
From: Richard Kleinhenz [mailto:scubaman@us.ibm.com]
Sent: 28 May 2002 19:11
To: Mike Groves
Cc: VEE Reflector (E-mail)
Subject: RE: vrf VEE 6.1



On my win2k system Help-About *DOES* indicate the correct version number
6.03.  6.01 was also indicated in the past.

But File Properties - Vesion for vee.exe tells me 6.0.1.0.  I don't know
which files the 601 to 603 update patched...

--
Regards,
Rich
===========================
Richard Kleinhenz
mailto:scubaman@us.ibm.com
845-892-2617
===========================




                      Mike Groves

                      <Mike.Groves@ultr        To:       "VEE Reflector
(E-mail)" <vrf@lvld.agilent.com>
                      arf.com>                 cc:

                      Sent by:                 Subject:  RE: vrf VEE 6.1

                      owner-vrf@lvld.ag

                      ilent.com





                      05/28/2002 01:19

                      PM








The thing I dislike about the VEE updates (including 6.01 & 6.03), is if
you have several development seats and a bunch of run-time machines, how
are you supposed to tell if any of the updates have been installed???
Have you noticed the version numbers don't change?

HELP/ABOUT gives the original "6.0 (Mar 27, 2000)" response.
PROPERTIES/VERSION of VEE.EXE and VEERUN60.DLL both still say "6.0".
whichversion() still says "6.0".

There's a very slight file size change (a few bytes) for each release so
I guess I will have to keep a table of file sizes vs. release numbers so
I can tell what version a particular machine is running. I haven't seen
6.1 yet so I can only hope the program responds with "6.1" when asked.

While I'm on the topic, I'd like to also include the manual sets that come
with the program. None that I've seen have any version numbers on them. I
can go to the bookshelf where they are kept and have to read into a manual
before I can determine what version it is. How hard can it be to add that
to the outside of the manuals? (I now have a big black marker that solves
that problem.)

(End ranting)

Mike Groves

-----Original Message-----
From: Rowe, Martin (Cahners) [mailto:m.rowe@tmworld.com]
Sent: Tuesday, May 28, 2002 8:08 AM
To: vrf@lvld.agilent.com
Subject: vrf VEE 6.1


I just heard from Agilent regarding VEE 6.1. They didn't send out press
releases for this "minor upgrade." I'll leave it to you users to decide
what's minor.

Martin Rowe
Senior Technical Editor
Test & Measurement World
+1-617-558-4426
m.rowe@tmworld.com
http://www.tmworld.com
(See attached file: att1a75r.dat)



---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address
"vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------





---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes