AnsweredAssumed Answered

vrf RS-485 RS232 over LAN

Question asked by VRFuser on Nov 13, 2002
Just got a MOXA Lan to serial box. It can do RS232,RS485,RS422 from one
unit! DE211 running under Win2000. Nice little box for under 150,
configurable serial coms anywhere on your LAN. It has a software driver to
create a virtual COM port on your PC, so send something to COM:8 and it
appears on the D type on the Moxa box somewhere else. So far great running
under 2K when you set the Agilent IO config for the vertual com port no
problem, but has anybody tried to set up virtual com ports in IO config
under 98 I get the error message that IO config has configured both COM1 &
Com2 so there are no more ports to config? (Its there and working from
windows)
Any thoughts great fully received.
Paul Rowan

BT Goonhilly
Tel :    +44 (0) 1872 325293
Fax :    +44 (0) 1872 325468
e-mail : paul.2.rowan@bt.com
http://www.satellite.bt.com
http://www.goonhilly.bt.com
> British Telecommunications plc
> Registered Office, 81 Newgate Street, London EC1A 7AJ
> Registered in England no 1800000
>
This electronic message contains information from British Telecommunications
plc, which may be privileged or confidential. The information is intended to
be for the use of the individual(s) or entity named above. If you are not
the intended recipient be aware that any disclosure, copying, distribution
or use of the contents of this information is prohibited. If you have
received this electronic message in error, please notify us by telephone or
email (to the numbers or address above) immediately.




-----Original Message-----
From: Schlieker, Reiner [mailto:reiner.schlieker@siemens.com]
Sent: 13 November 2002 14:01
To: VEE vrf
Subject: [vrf] RE: RS-485


I use the B&B Electronics 3PCISD4A card.  It fabulous: it's a 4 port card,
with each port individually configurable to RS232, RS422, or RS485, and it
just looks like 4 extra comm ports on your PC.  It's also quite fast,
supporting 460.8 kbps.  Check it out...
http://www.bb-elec.com/productlist.asp?Dept_id=171

Reiner


-----Original Message-----
From: Breitenbach, Richard [mailto:RBreitenbach@PanAmSat.com]
Sent: Wednesday, November 13, 2002 1:43 AM
To: VEE vrf
Subject: [vrf] RS-485


I plan on installing a serial RS-485 card in a PCI slot of PC and was
wondering if someone can recommend a card they might have used.  Looking for
one that I/O Config will detect with no problems and works using direct I/O
function of VEE.

Richard @
PanAmSat


---
You are currently subscribed to vrf as: reiner.schlieker@siemens.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com".

If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: paul.2.rowan@bt.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com".

If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes