<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 5.00.3315.2870" name=GENERATOR></HEAD><BODY><DIV><DIV><FONT size=2><FONT face=Arial><SPAN class=631322814-07082003><SPAN class=853594314-07082003>I</SPAN> need to be able to call a stored procedure from within VEE using an ADO, DAO, or RDO object (whatever works best) that will send 20 parameters and their values and will return one value from <SPAN class=853594314-07082003>a</SPAN><SPAN class=853594314-07082003> </SPAN>database<SPAN class=853594314-07082003> o</SPAN><SPAN class=853594314-07082003>n our network</SPAN>. The one value that will be returned from the database using the stored procedure is the EventID which is used to tie all the data together from the conditions and data tables. This procedure ensures the assignment of a unique test event id for a given set of results within the database.<SPAN class=853594314-07082003> </SPAN></SPAN></FONT></FONT></DIV><DIV><FONT size=2><FONT face=Arial><SPAN class=631322814-07082003><SPAN class=853594314-07082003></SPAN></SPAN></FONT></FONT> </DIV><DIV><FONT size=2><FONT face=Arial><SPAN class=631322814-07082003><SPAN class=853594314-07082003>Does anyone have any experience with something like this? Any help would be greatly appreciated.</SPAN></SPAN></FONT></FONT></DIV><DIV><SPAN class=631322814-07082003><SPAN class=853594314-07082003><P><FONT face=Arial size=2>Dwayne Rowland <BR><SPAN class=853594314-07082003>Sr. RF </SPAN>Technician <SPAN class=853594314-07082003>/ PA Applications</SPAN><BR>RF Micro Devices <BR>7625 Thorndike Rd. <BR>Greensboro, NC 27409 <BR>e-mail: drowland@rfmd.com </FONT></P></SPAN></SPAN></DIV><DIV><SPAN class=631322814-07082003></SPAN><FONT face=Arial size=2> </FONT></DIV></DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@it.lists.it.agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>