AnsweredAssumed Answered

vrf Problem with Real32 data constant

Question asked by VRFuser on Sep 6, 2006
Hi All,

    I have a persistent problem with all of my VEE programs to date.  The problem is that when I use a Real32 data constant on the front panel of a user object, VEE seems to put a lot of additional numbers behind the decimal.  For example, if I want to input say 1.25, then the next time I run the program and want to change this, I click on the Real32 data constant and it has something like 1.250000688493.  Why is this? And how can I stop it from happening? 

   For more information, the user object is there to load in parameters from a file for the current experiment I am doing, and then save them after a change and proceed with the rest of the experiment.  When I save the parameters, I edit the transaction so it only saves in Fixed format, with say 4 numbers after the decimal, however on running the program again, it still has the problem.

    Many thanks

Duncan

--

Duncan Wild
Max-Planck-Institut für biophysikalische Chemie
Abteilung Spektroskopie und Photochemische Kinetik (10100)
Am Faßberg 11
D-37077 Göttingen
GERMANY
 
Tel.:     +49-551-201-2004 (Office)
Tel.:     +49-551-201-1775 (Lab)
FAX :     +49-551-201-1501
E-mail:   HYPERLINK "mailto:dwild@gwdg.de"dwild@gwdg.de
-------------------------------------------------------

 


---

To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".  

Outcomes