AnsweredAssumed Answered

vrf font size

Question asked by VRFuser on Jul 29, 2003
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 5.00.3315.2870" name=GENERATOR></HEAD><BODY><DIV> </DIV><BLOCKQUOTE style="MARGIN-RIGHT: 0px">  <P><FONT color=#0000ff face=Arial size=2><SPAN class=841163311-30072003>I have   seen programs that use a font size of 10 as the Default Font value. When I go   into the Default Preferences to change the default font size it does   absolutely nothing. Is there another way to change the default font size so   that all objects in the program, formulas, Direct I/Os, etc., have a different   default font value than 12?</SPAN></FONT></P>  <P><FONT color=#0000ff face=Arial size=2><SPAN   class=841163311-30072003></SPAN></FONT> </P>  <P><FONT color=#0000ff face=Arial size=2><SPAN   class=841163311-30072003>Dwayne</SPAN></FONT></P></BLOCKQUOTE>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>  

Outcomes