AnsweredAssumed Answered

vrf FW: Folder browsing (Multiple files)

Question asked by VRFuser on Jun 27, 2003
Thank you for your quick response. The solution is pretty cool and works
great. I will apply your solution to my program. But I still have question
why VEE didn't handle that or maybe this can be considered as bug.

Thanks again.

----- Original Message -----
From: <Peter_M_Fender@raytheon.com>
To: "VEE vrf" <vrf@it.lists.it.agilent.com>
Cc: "Cagri Acar" <cacar@aselsan.com.tr>
Sent: Friday, June 27, 2003 3:44 PM
Subject: [vrf] Re: Address of Spoll Object


>
> I use a 'dummy' instrument with a short timeout (1 sec) that I can change
> the address on, and then SPOLL it.
> See enclosed.
>
> Peter Fender
> Raytheon Network Centric Systems
> St. Petersburg, FL.
>
> (See attached file: Addressable SPOLL.vee)
>
>
>
>
>
>
> Hello everybody,
> Did anyone notice that we cannot create an address input to the SPOLL
> object. I want my device io functions to have address inputs so that I can
> dynamically change the address of the instruments (I think this may work
> while two instruments of the same kind are working simultaneously with the
> same functions). But I was not able to create the input for the SPOLL
> object. Am I missing something about SPOLL or is this a bug?
>
> Regards
>
> Cagri ACAR
> Test Engineer
> Microwave Systems Technologies Test Engineering Department
> ASELSAN AS
> PK101 Yenimahalle 06370 ANKARA TURKEY
> Phone: +903125922228
>
>
>


----------------------------------------------------------------------------
----


> ---
> You are currently subscribed to vrf as: cacar@aselsan.com.tr
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email
"vrf@it.lists.it.agilent.com".
> If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
>


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes