AnsweredAssumed Answered

vrf Isolating Program Flow

Question asked by michael.asbery on Jul 15, 2003

Shawn,
Please examine my 'do nothing' loop.  When it is doing nothing, it does
indeed have a 1 second delay, which releases 99.999% of the processing
time.  When it is looping, the delay isn't used.

Regards

Dave




                      "Shawn Fessenden"
                      <shawn@testech-lt        To:       "VEE vrf" <vrf@it.lists.it.agilent.com>
                      d.com>                   cc:
                                               Subject:  [vrf] RE: Pause function
                      16-Jul-2003 04:06
                      PM
                      Please respond to
                      "Shawn Fessenden"






Dave,

> Does anyone know how to create a pausing
> function in HP-VEE

Though there are many ways to do so, you're probably better off using a
Delay object than constructing a do-nothing loop. The problem with a
do-nothing loop is that it doesn't do nothing, it eats CPU cycles that can
be put to better use elsewhere. Of course, if your design is a VEE only
system, that's no big deal, but if the computer is running other
applications VEE can get to be a real CPU hog.
-SHAWN-


---
You are currently subscribed to vrf as: Dave.Watling@Zarlink.Com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email
"vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".






---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes