Hello detlef,
this is the solution for today. Thank you.
I will try the two instances of VEE.
regards,
Horst
-----Ursprngliche Nachricht-----
Von: Baranski, Detlef [mailto:Detlef.Baranski@PILKINGTON.de]
Gesendet: Donnerstag, 3. April 2003 15:18
An: VEE vrf
Cc: 'Kunkel, Horst'
Betreff: [vrf] Printer scaling and orientation at runtime?
Hello list,
i did have similar problem in the past and got the following hint from
Agilent:
1. basic problem is windows itself as it uses just one printer during one
session.
With Vee you can declare one printer with orientation and scaling which fits
to your needs.
2. If you need different outputs (print designs), the only chance you have
is to use a new vee program with a different "standard printer design". Then
you can call the Vee-No2 program from Vee-No1 program and so on.
I did try to use some Windows library functions according to the microsoft
help list, but it does not change the standard printer during vee runtime. I
think the solution above is currently the only one i have heard of. I also
hope to get new infos and maybe some update with better support in that area
from Agilent.
My problem was that i wanted to print my data on paper and simultanously as
a pdf file with Acrobat. Now you can get a program for 50 Euro which did it
automatically, but in the past the run of 2 vee sessions was the only
solution for that.
As i am a " rookie " on this list, i apologyse for possible mistakes ;.)
Best regards,
detlef
-----
-----Ursprngliche Nachricht-----
Von: Kunkel, Horst [mailto:Kunkel@hansa.de]
Gesendet: Mittwoch, 2. April 2003 17:21
An: VEE vrf
Betreff: [vrf] AW: printer scaling and orientation at runtime?
Hello B. Aufenanger,
thanks for your response. But (hello agilents =:o)this is solid work down to
the roots
of printing. In my opinion it should be possible to print e.g. images
and graphs stored within different panels independent from the orientation
and dimensions of that panel just by scaling and rotating
it programmatically. It seems that at runtime by no means not even changing
of the
printer is possible, its always the standard printer at start up of the
program. Or have I overlooked something?
regards
Horst
-----Ursprngliche Nachricht-----
Von: B Aufenanger [mailto:aufenanger@somatec.de]
Gesendet: Mittwoch, 2. April 2003 14:01
An: VEE vrf
Betreff: [vrf] AW: printer scaling and orientation at runtime?
Use the "toFile" object instead of the "toPrinter" object. Then you are able
to send the escape sequences to your printer.
Best regards
B. Aufenanger
------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen
Telefon : (089) 613 984 91
Fax. : (089) 613 981 23
Email : mailto:Aufenanger@somatec.de
homepage : http://www.somatec.com/
------------------------------------------------------------
-----Ursprngliche Nachricht-----
Von: Kunkel, Horst [mailto:Kunkel@hansa.de]
Gesendet: Dienstag, 1. April 2003 08:59
An: VEE vrf
Betreff: [vrf] printer scaling and orientation at runtime?
Hello vrf users,
does anybody know if there is any solution to change orientation and scaling
of a function
panel printout at runtime? Selectable by the user or simply by the program
if appropriate?
Is it possible to get rid of the unwished time stamp on the printout?
Greetings
Horst
______________________________________________________________________
This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.
Visit our internet site at http://www.pilkington.com
---
You are currently subscribed to vrf as: L.Smidt@GeoDelft.nl
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
this is the solution for today. Thank you.
I will try the two instances of VEE.
regards,
Horst
-----Ursprngliche Nachricht-----
Von: Baranski, Detlef [mailto:Detlef.Baranski@PILKINGTON.de]
Gesendet: Donnerstag, 3. April 2003 15:18
An: VEE vrf
Cc: 'Kunkel, Horst'
Betreff: [vrf] Printer scaling and orientation at runtime?
Hello list,
i did have similar problem in the past and got the following hint from
Agilent:
1. basic problem is windows itself as it uses just one printer during one
session.
With Vee you can declare one printer with orientation and scaling which fits
to your needs.
2. If you need different outputs (print designs), the only chance you have
is to use a new vee program with a different "standard printer design". Then
you can call the Vee-No2 program from Vee-No1 program and so on.
I did try to use some Windows library functions according to the microsoft
help list, but it does not change the standard printer during vee runtime. I
think the solution above is currently the only one i have heard of. I also
hope to get new infos and maybe some update with better support in that area
from Agilent.
My problem was that i wanted to print my data on paper and simultanously as
a pdf file with Acrobat. Now you can get a program for 50 Euro which did it
automatically, but in the past the run of 2 vee sessions was the only
solution for that.
As i am a " rookie " on this list, i apologyse for possible mistakes ;.)
Best regards,
detlef
-----
-----Ursprngliche Nachricht-----
Von: Kunkel, Horst [mailto:Kunkel@hansa.de]
Gesendet: Mittwoch, 2. April 2003 17:21
An: VEE vrf
Betreff: [vrf] AW: printer scaling and orientation at runtime?
Hello B. Aufenanger,
thanks for your response. But (hello agilents =:o)this is solid work down to
the roots
of printing. In my opinion it should be possible to print e.g. images
and graphs stored within different panels independent from the orientation
and dimensions of that panel just by scaling and rotating
it programmatically. It seems that at runtime by no means not even changing
of the
printer is possible, its always the standard printer at start up of the
program. Or have I overlooked something?
regards
Horst
-----Ursprngliche Nachricht-----
Von: B Aufenanger [mailto:aufenanger@somatec.de]
Gesendet: Mittwoch, 2. April 2003 14:01
An: VEE vrf
Betreff: [vrf] AW: printer scaling and orientation at runtime?
Use the "toFile" object instead of the "toPrinter" object. Then you are able
to send the escape sequences to your printer.
Best regards
B. Aufenanger
------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen
Telefon : (089) 613 984 91
Fax. : (089) 613 981 23
Email : mailto:Aufenanger@somatec.de
homepage : http://www.somatec.com/
------------------------------------------------------------
-----Ursprngliche Nachricht-----
Von: Kunkel, Horst [mailto:Kunkel@hansa.de]
Gesendet: Dienstag, 1. April 2003 08:59
An: VEE vrf
Betreff: [vrf] printer scaling and orientation at runtime?
Hello vrf users,
does anybody know if there is any solution to change orientation and scaling
of a function
panel printout at runtime? Selectable by the user or simply by the program
if appropriate?
Is it possible to get rid of the unwished time stamp on the printout?
Greetings
Horst
______________________________________________________________________
This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.
Visit our internet site at http://www.pilkington.com
---
You are currently subscribed to vrf as: L.Smidt@GeoDelft.nl
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
I'm trying to update a strip chart graph. I want 2 traces. Trace one is
the desired temperature profile of a chamber for a 24 hour period. This
profile starts at 25C, ramps up to 65C, stays at 65C for x hours, ramps
down to 25C, ramps back to 65, stay at 65 for x hours, ramp down to 25C,
stay at 25C for x hours, ramp down to -10C, stay at -10C for x hours, ramp
back to 25C: End of 24 hour period.
I can graph the desired profile, but when I try to add trace 2 (the actual
temp of the chamber), I get a flat horizontal line at that temp, not a 2nd
trace overlayed on the 1st.
I'm trying to show progress in the profile. I'd even consider using one of
the markers to show current location in my profile, but I can't see where I
input where I want the markers.
Any ideas?
Thanks
Tom Mitchell
Autoliv
AEA
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".