AnsweredAssumed Answered

vrf Excel ActiveX problem

Question asked by VRFuser on Nov 12, 2001
Thanks for the help.

I have one small problem left, actually I have two.

First problem:
When excel starts up, and the sheets are created the "save as" buttom is
crayed out the only thing I can do if I want to save the sheet from excel is
to select "Save copy as"

I know there is a method to save the sheets from VEE, but I would like to be
able to save the sheets from Excel.

Second problem:
If I close down VEE after the sheets have been created, Excel closes as
well, how do I avoid this.

Thanks in advance

Kenth Jensen


-----Original Message-----
From: ext Markus Bernhardt [mailto:Bernhardt@somatec.de]
Sent: 12 november, 2001 13:23
To: 'Kenth.Jensen@nokia.com'
Cc: VEE Usergroup (E-Mail)
Subject: AW: vrf Excel ActiveX problem


Hi Kenth,

you have to specify the sheet like:

<<vee-excel.vee>>

Best regards

M. Bernhardt
-----------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen

Telefon     : (089) 613 984 94
Fax         : (089) 613 981 23
Email       : mailto:Bernhardt@somatec.de
Homepage    : http://www.somatec.com/
-----------------------------------------


-----Ursprngliche Nachricht-----
Von:      owner-vrf@lvld.agilent.com [mailto:owner-vrf@lvld.agilent.com]  Im
Auftrag von Kenth.Jensen@nokia.com
Gesendet:     Montag, 12. November 2001 09:45
An:     vrf@lvld.agilent.com
Betreff:     vrf Excel ActiveX problem

<< Datei: vee-excel.vee >> Hi

Im having some problems with the attached program.

Im adding one sheet extra sheet in excel, but I cant control what sheet im
writing in.

I try to select the sheet I want to write in before I start writing, but it
writes in the wrong sheet.

How do I control this.

Im using Excel ver 97.

Regards
Kenth Jensen

<<vee-excel.vee>>
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes