Hi,
I know there is an IO ActiveX Control written by J.S.Payne that embeds into Vee quite nicely.
Go to http://www.jspayne.com/
Best Regards,
James
-------------------------------------------------------
James Atkin BEng(Hons) AMIEE
Software Engineer
Mitec Telecom Ltd
The Arenson Centre
Arenson Way
Dunstable
Bedfordshire
LU5 5UL
-------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.agilent.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
I know there is an IO ActiveX Control written by J.S.Payne that embeds into Vee quite nicely.
Go to http://www.jspayne.com/
Best Regards,
James
-------------------------------------------------------
James Atkin BEng(Hons) AMIEE
Software Engineer
Mitec Telecom Ltd
The Arenson Centre
Arenson Way
Dunstable
Bedfordshire
LU5 5UL
-------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.agilent.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
Best regards
Ralf
***********Source: MSDN
Library*************************************************************************************************************************
PRB: Using the Internet Transfer Control on an ASP Page
ID: Q216288
--------------------------------------------------------------------------------
The information in this article applies to:
Microsoft Visual Basic Learning, Professional, and Enterprise Editions for
Windows, versions 5.0, 6.0
Microsoft Internet Information Server versions 4.0, 5.0
--------------------------------------------------------------------------------
SYMPTOMS
When using the Internet Transfer Control on an Active Server Pages (ASP) page
that has been deployed on a remote
Web server and the remote Web server does not have Visual Basic installed, the
following error message occurs
when accessing the ASP page:
Server object error 'ASP 0177 : 80040112'
Server.CreateObject Failed
/WebAppRoot/ASPPage.asp, line xx
CAUSE
This problem occurs because the Internet Transfer Control is a licensed control
and ASP page does not have the
mechanisms to invoke the License Manager for the licensed control.
RESOLUTION
To resolve this problem, encapsulate the ActiveX control in an in-process,
ActiveX component (a dynamic-link library,
or DLL) that allows the Internet Transfer Control to be redistributed and allows
the deployment of the control to the remote
Web server.
The following instructions demonstrate how to encapsulate the Internet Transfer
Control within a Visual Basic in-process,
ActiveX component:
Open Visual Basic and create a New Project.
In the New Project dialog box, select ActiveX DLL and click Open.
In the Project window, right-click Project1 and click Add.
In the Add Form dialog box, select Form and click Open.
Add the Internet Transfer Control to the toolbox. From the Project menu, click
Components. In the Components
dialog box, select the Microsoft Internet Transfer Control 6.0. Click OK.
Add the Internet Transfer Control to the Form. From the Toolbar, click the Inet
control and add the control onto the form.
Now, open Class1 in the Class Module folder under Project1 and add the following
code to Class1:
Private objForm As Object
Private Sub Class_Initialize()
Set objForm = New Form1
End Sub
Public Function OpenURL(strURL As String)
OpenURL = objForm.Inet1.OpenURL(strURL)
End Function
Public Property Let RequestTimeOut(intRTO As Integer)
objForm.Inet1.RequestTimeOut = intRTO
End Property
Public Property Get RequestTimeOut() As Integer
RequestTimeOut = objForm.Inet1.RequestTimeOut
End Property
Save the project. From the File menu, click Save Project.
Compile the project into a DLL. From the File menu, select Make Project1.dll.
After you create and compile the ActiveX DLL, you can deploy it and the Internet
Transfer Control to the remote
Web server. The following steps describe how to deploy the ActiveX DLL and the
Internet Transfer Control to a remote
Web server.
Copy the Msinet.ocx to the remote Web server. You can copy the ActiveX control
to any directory.
Also, copy the ActiveX DLL (Project1.dll) to the remote Web server. Place it in
the same location as the Msinet.ocx.
Register the ActiveX control and the ActiveX DLL using RegSvr32.exe. To register
the control and the DLL, click the
Start button and select Run. In the Run box, enter cmd to bring up the Command
window. In the Command window,
change to the directory where the control and DLL reside and register the
components as shown below:
Regsvr32 MSINET.OCX [Enter]
Regsvr32 Project1.dll [Enter]
To test the ActiveX control and ActiveX DLL, use the following server-side
Visual Basic Script (VBScript) on an
ASP page. You can use Visual InterDev to create the ASP page.
<%@ Language="VBScript" %>
<%
Response.Buffer = true
set objInetTransCtrl = Server.CreateObject("Project1.Class1")
strPage = objInetTransCtrl.OpenURL("http://msdn.microsoft.com/vinterdev")
'substitute your URL here
Response.Write strPage
%>
This sample ASP page instantiates the encapsulated control and renders the home
page from Visual InterDev Web site on the browser.
STATUS
This behavior is by design.
MORE INFORMATION
Using the Internet Transfer Control or any other ActiveX controls on an ASP page
with server-side script is not supported
by Microsoft. ActiveX controls are designed to be run on a client application
such as a Web browser (Internet Explorer)
or on a Visual Basic form. These controls have events that may require user
interaction. Since ASP is processed on
the Web server, there is no user interaction to respond to these events when
the events are executed by the controls.
Hence, other issues may occur when the controls execute their events and require
user interaction.
If this should happen with the encapsulated Internet Transfer Control on an ASP
page, you may have to create
another ActiveX component that uses the WinInet Application Program Interface
(API).
REFERENCES
Please refer to the following Web sites for more related information:
http://msdn.microsoft.com/vinterdev/
http://msdn.microsoft.com/vbasic/
Additional query words:
Keywords : kbActiveX kbASP kbVBp600 kbGrpASP kbiis400 kbiis500
Version : WINDOWS:5.0,6.0
Platform : WINDOWS
Issue type : kbprb
Technology :
Last Reviewed: December 8, 1999
2000 Microsoft Corporation. All rights reserved. Terms of Use.
********************************************************************************************************************************************************
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.agilent.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------