AnsweredAssumed Answered

vrf The invisible object...

Question asked by VRFuser on Dec 10, 2002
Cool, it works exactly as you described.
Nice bug also in VEE6.03

Christian


From:                Jonas Frisk <Jonas.Frisk@lgp.se>
To:                  "VEE vrf" <vrf@it.lists.it.agilent.com>
Subject:             [vrf] The invisible object...
Date sent:           Wed, 11 Dec 2002 12:31:33 +0100
Send reply to:       Jonas Frisk <Jonas.Frisk@lgp.se>

> Has anybody seen my message box?
>
> I've stumbled on an small problem today using VEE 6.0 and I've also seen the
> problem using VEE 5.0 but the problem seem to get worse in the newer
> version.
>
> Try creating a Message Box (Data/Dialog Box). Set the "Buttons" to "OK" and
> enable the "Timeout" on the object properties. You'll get a message box
> object with two data outputs, "OK" and "Timeout". Now try to change the
> "Buttons" to "OK Cancel" and whops the "Timeout" output disappears and is
> replaced with the "Cancel" output. Now try to disable the "Timeout" and an
> error message should appear and the object should disappear
>
> Now you'll have an empty work area but take a closer look to the area where
> the message box object was before. Try scrolling the worka area by LMB
> clicking on this area and moving the mouse cursor. Also try to use the
> multiple select function using this area as a starting point (pressing Ctrl
> and LMB and moving the mouse cursor). The latter will result in an ordinary
> clone object.
>
> The problem is easily solved by closing and reopening the .vee file or you
> can try cutting the invisible object using different cut commands depending
> on VEE version.
>
> Strange???
>
> // Jonas Frisk
>
>
> ---
> You are currently subscribed to vrf as: Christian.Wienhold@biotronik.de
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com".
> If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
>


BIOTRONIK GmbH & Co.
EWE 51/CW
D 12359 Berlin - Neuklln
Tel.: +49 30 689 05 - 301
--------------------------------------
christian.wienhold@biotronik.de
--------------------------------------





---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes