<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2713.1100" name=GENERATOR></HEAD><BODY style="MARGIN-TOP: 2px; FONT: 8pt Tahoma; MARGIN-LEFT: 2px"><DIV><FONT size=1>Has anyone used the Kernel32.dll to find what drives are available. I have only had luck with the A: drive being returned as available.</FONT></DIV><DIV><FONT size=1></FONT> </DIV><DIV><FONT size=1>Thanks in advance.</FONT></DIV><DIV><FONT size=1></FONT> </DIV><DIV><FONT size=1></FONT> </DIV><DIV><FONT size=1>Bob</FONT></DIV><DIV> </DIV><DIV><FONT size=1>Robert Rais<BR>Engineer<BR>Yazaki North America Inc.<BR>Testing and Reliability<BR><A href="mailto:rrais@yazaki-na.com">rrais@yazaki-na.com</A><BR>*Direct:734-983-6444<BR> Fax: 734-983-6445</FONT></DIV></BODY></HTML>
A READ TEXT transaction with STRING format will read one line of a file. Use
the word null for the data field when editing the transaction and the From
File object won't even create an output.
Regards,
Bill Ossmann
--
bill_ossmann@hsgmed.com
Philips Ultrasound
>-----Original Message-----
>From: Bill Blore [mailto:BBlore@EXCALIBUR.com]
>Sent: Monday, March 25, 2002 9:44 AM
>To: vrf@lvld.agilent.com
>Subject: vrf Read file and reject first 5 lines.
>
>
>I am sure there is an easy way to do this. I need to parse a
>data file and
>reject the first n lines, and then read the rest of the data.
>
>Bill Blore
>email: bblore@excalibur.com
>phone: 1 613 591 5675 x 215
>fax: 1 613 591 6001
>Toll Free: 1 800 667 8807
>50 HInes Road, Kanata, Ontario, Canada K2K 2M5
>Web Site: www.excalibur.com
> <<Bill Blore.vcf>>
>
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.agilent.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------