AnsweredAssumed Answered

vrf Problem with FlashWindow using Windows API

Question asked by VRFuser on Sep 25, 2001
How stupid of me not to look in the examples.

Thanks for all the help to everybody.

Regards
Kenth

-----Original Message-----
From: ext Pickles, Warren [mailto:picklesw@tycoelectronics.com]
Sent: 26 september, 2001 9:08
To: vrf@lvld.agilent.com; Jensen Kenth (NMP/Copenhagen)
Subject: RE: vrf Problem with FlashWindow using Windows API


There's an example that comes with VEE Pro 6.  Help ... Open example ...
then look in contribWin32Api
Cheers,
Warren Pickles



-----Original Message-----
From: sander.wubbels@philips.com [mailto:sander.wubbels@philips.com]
Sent: 26 September 2001 07:29
To: Kenth.Jensen@nokia.com
Cc: vrf@lvld.agilent.com
Subject: Re: vrf Problem with FlashWindow using Windows API



Kenth,

You can use one of the following APIs:

long _stdcall GetActiveWindow ();
long _stdcall FindWindowA (long lpClassName, char* lpWindowName);

Both return a HWnd. Use this as input of your flashwindow.

Hope this helps,

-------------------------------------------------------------------------
       S. Wubbels
       Test Engineer

                MST - Personal Communications
                Philips Semiconductors
                Gerstweg 2 Nijmegen
                Tel.: (+35) (0)24 353 29 90
                E-mail: Sander.Wubbels@philips.com
-------------------------------------------------------------------------





Kenth.Jensen@nokia.com@lvld.agilent.com on 26/09/2001 08:17:35

Sent by:  owner-vrf@lvld.agilent.com


To:     vrf@lvld.agilent.com
cc:      (bcc: Sander Wubbels/NYM/SC/PHILIPS)
Subject:  vrf Problem with FlashWindow using Windows API
Classification:



Hi

I have been trying to use the FlashWindow Function in the Windows API
without any luck.
My problem is that the first input in the call to the function (hwnd) should
be a handle to the window to flash, and I dont know what data to put on that
input.
See attached file.
<<FlashWindow.vee>>
I have found some documentation on the FlashWindow Function on the adress
below, without any improvements.
http://www.vbapi.com/ref/f/flashwindow.html

Could anyone please help me out on this one.

Regards

Kenth Jensen
Nokia Mobile Phones
Copenhagen








---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes