<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2600.0" name=GENERATOR><STYLE></STYLE></HEAD><BODY bgColor=#ffffff><DIV><FONT face=Arial size=2>I have looked at the ReadMarkerValue example in VEE. It seems that as long as the mouse button is pushed the marker displays are not updated. Is there a way to update the marker readouts while the markers are being moved?</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><FONT face=Arial size=2>Hal Cornelius</FONT></DIV></BODY></HTML>