AnsweredAssumed Answered

vrf SCPI driver problem

Question asked by VRFuser on Apr 28, 2002
Dear all,

I-SCPI has solved the problem. I' ll also move to P&P as soon as possible.
Thank you for your interest.

Cem Kayis

----- Original Message -----
From: "M Watts" <MikeJWatts@compuserve.com>
To: "Cem Kayis" <kayis@aselsan.com.tr>
Cc: "[unknown]" <vrf@lvld.agilent.com>
Sent: Saturday, April 27, 2002 1:25 AM
Subject: vrf SCPI driver problem


> Erm, the version of IO Libs I have ( yes its 'J' but its not that old )
has
> an entry for I-SCPI.  To add it you go to the IO Config applet, click on
> the I-SCPI in the 'Available Interfaces' list and 'Add'.  That should do
> the trick.
>
> Having said that, it seems that Jay Nemeth-Johannes is 'the reference' to
> have on this, so if he says you can't do it then I am not going to argue!
> It would seem that even if you can do direct I/O using I-SCPI, you won't
be
> able to do it in future, so this will cause some support headaches.
>
>
>
> Mike Watts
>
>
>
> _______________________________________________________________________
>
>   Michael Watts, Consultant                                 PO Box 92
>   on the web: www.PreciselySo.Co.UK                      Exeter,Devon
>   e-mail: MJWC@PreciselySo.Co.UK                              England
>   tel: +44 7714 339 729                                       EX4 2YY
> _______________________________________________________________________
> ---------------------------------------------------------------------
> This is the "vrf" maillist, managed by Majordomo.  To send messages to
> this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
> unsubscriptions are done through the address
"vrf-request@lvld.agilent.com".
> If you need details, just send a message containing the text "help"
> to "vrf-request@lvld.agilent.com".
> ---------------------------------------------------------------------

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes