<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><XETA content="text/html; charset=iso-8859-9" http-equiv="Content-Type"><XETA content="MSHTML 5.50.4807.2300" name="GENERATOR"><STYLE></STYLE><META content="MSHTML 6.00.2715.400" name=GENERATOR></HEAD><BODY bgColor=#ffffff><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002>The MATLAB Script will not be able to use M-files. The only way that I know of is to use MATLAB's development environment to create P-files ('compiled' M-files). These can then be used by MATLAB Script. This has to do with how The Mathworks setup MATLAB Script engine to work.</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002>But if/since you have MATLAB 5.1 you can easily create P-files using the pcode command.</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002></SPAN></FONT> </DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002>//</SPAN></FONT></DIV><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002></SPAN></FONT><FONT face=Arial color=#0000ff size=2><SPAN class=328455214-16042002><FONT face=Arial size=2>Gran Johnsson</FONT> <BR><FONT face=Arial size=2>Technical Consultant - Test Automation<B></B></FONT> </DIV><DIV><P><FONT face=Arial size=2>Agilent Technologies</FONT> <BR><FONT face=Arial size=2>P.O. Box 52</FONT> <BR><FONT face=Arial size=2>Kronborgsgrnd 23</FONT> <BR><FONT face=Arial size=2>164 94 Kista</FONT> <BR><FONT face=Arial size=2>Sweden</FONT> <BR><FONT face=Arial size=2><I> </I></FONT><BR><FONT face=Arial size=2>Tel: +46 (8) 5064 8789</FONT> <BR><FONT face=Arial size=2>Fax: +46 (8) 5064 8616</FONT> <BR><FONT face=Arial size=2>Mobile: +46 (70) 325 2089</FONT> <BR><FONT face=Arial size=2>Email: goran_johnsson@agilent.com</FONT> <BR><FONT face=Arial size=2>Web: <A href="http://www.agilent.com/" target=_blank>http://www.agilent.com</A></FONT> <BR><FONT face=Arial size=2>Intranet: <A href="http://tmsw.sweden.agilent.com/" target=_blank>http://tmsw.sweden.agilent.com</A></FONT> </P><BR><BR></SPAN></FONT></DIV><BLOCKQUOTE dir=ltr style="PADDING-LEFT: 5px; MARGIN-LEFT: 5px; BORDER-LEFT: #0000ff 2px solid; MARGIN-RIGHT: 0px"> <DIV class=OutlookMessageHeader dir=ltr align=left><FONT face=Tahoma size=2>-----Original Message-----<BR><B>From:</B> Cengiz Eken [mailto:ceken@aselsan.com.tr]<BR><B>Sent:</B> Monday, April 15, 2002 13:09<BR><B>To:</B> vee_user_group<BR><B>Subject:</B> vrf MATLAB together with VEEPro<BR><BR></FONT></DIV> <DIV><FONT face=Arial size=2>Dear All,<BR>We have a problem on using already installed Matlab5.1 together with VEE6.01.<BR>For this case I shouldn't have any problem on using Matlab according to the Agilent VEE Pro's Help. But when we run a VEE program that contains Matlab Script and this script calls a Matlab .m file(s), we have a "VEE Run Time Error" as below. </FONT></DIV> <DIV> </DIV> <DIV><FONT face=Arial size=2>"Matlab Script Execution Error<BR>Matlab Error Message. Error loading *.m<BR>M-files cannot be run in Runtime Matlab.<BR>Error number: 593."</FONT></DIV> <DIV> </DIV> <DIV><FONT face=Arial size=2>It is stated in the "Multiple MATLAB Versions" part of the "Matlab Script" help that :<BR>"Before VEE uses the MATLAB Script engine, it checks if MATLAB is already registered on the system. If MATLAB is already present, the MATLAB Script engine installed with VEE is not registered as the MATLAB Automation Server. In this case, VEE uses the existing MATLAB and does not interfere with the operation of the MATLAB development environment."</FONT></DIV> <DIV> </DIV> <DIV><FONT face=Arial size=2>If VEE uses the existing Matlab why do we have this problem? What can you suggest to use existing MATLAB 5.1 with VEE6.01?<BR>Regards<BR>Cengiz Eken<BR>Sr.Test Engineer</FONT></DIV></BLOCKQUOTE></BODY></HTML>
b) what is the question?
-----Original Message-----
From: Gregg C Levine [mailto:hansolofalcon@worldnet.att.net]
Sent: Saturday, 13 April 2002 21:23
To: Vrf
Subject: vrf Sockets, and VEE and two computers
Hello from Gregg C Levine normally with Jedi Knight Computers
I have just completed a simple test to enable sending of data between
two computers running VEE, this one, named "Who", and the other one,
named, "Spock". I used on this machine a simple socket object, with one
data input point, and two data outpoints, and the same arrangement on
the other. After a reasonable delay, caused my guess by the way Windows
does its networking, the whole thing worked. This is VEE Pro 6.01, and
with the version L 1.0.0 of the IO drivers installed. And it was
installed on both machines. The IP addresses, and machine names were
resolved using simple DHCP arrangements, and the network cards were 3COM
3C905Cs. Right now I am endeavoring to add the IO objects to this one,
but to accept data via that socket object from the other.
-------------------
Gregg C Levine hansolofalcon@worldnet.att.net
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.agilent.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------