<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2600.0" name=GENERATOR><STYLE></STYLE></HEAD><BODY bgColor=#ffffff><DIV><FONT face=Arial size=2><DIV><FONT face=Arial size=2>A few questions.</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><DIV><FONT face=Arial size=2>Is it possible to have different color values for each marker when you have two markers on a display object? </FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><DIV><FONT face=Arial size=2>Also, I have looked at the ReadMarkerValue example in VEE. It seems that as long as the mouse button is pushed the marker displays are not updated and the VEE program stops. And there is a position output on the display object that shows the XY position of the mouse pointer that changes with the mouse movement. Is there a way to get the marker readouts while the markers are being moved? And keep processing VEE threads in the background?</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><FONT face=Arial size=2>Hal Cornelius</FONT></DIV><DIV><FONT face=Arial size=2>Hi-Val-U Associates</FONT></DIV></DIV></DIV></FONT></DIV></BODY></HTML>