AnsweredAssumed Answered

vrf Active X - common dialogue

Question asked by VRFuser on Feb 13, 2002
It may need to be registered, this is done automaticaly on your machine if
you install VB, but when installing on another 98 machine that has not had
an application loaded that registers the control I have used
"c:windowssystem
egsvr32 ******.ocx" it may be simalar with DLL's
Regards
Paul

-----Original Message-----
From: Ivan Edwards [mailto:ivan.edwards@irisys.co.uk]
Sent: 14 February 2002 09:53
To: 'vrf@lvld.agilent.com'
Subject: vrf Active X - common dialogue


I have just loaded Vee6.01 Pro on my PC which has windows millenium edition.
On opening the AxtiveXControls example CommonDialog, I get the Vee Caution,

Could not load the following Active X reference:
Microsoft Common Dialog Control 5.0
Version 1.0

Verify you have the required ActiveX component properly installed on this
system.

The program then opens and there is a note pad warning that comdlg32.ocx
needs to be installed for the program to work.  On searching my
c:windowssystem I can see this file and it's associated .dll listed.  How
do I get it recognised by the system?
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes