AnsweredAssumed Answered

vrf Vee Requests ...

Question asked by VRFuser on Jan 14, 2003
Hi all,

I have submitted several 'suggestions' in the past via the Agilent Web
Site, but as yet, I have not received any reply on :
  1. If these requests are being considered
  2. How many other people have made a similar request
  3. What other requests have been made

I understand that it is difficult for Agilent to let the users know
what requests are being considered. There is always the chance that they
even though they are being considered, they might not make it as part of
the next release; and of course if this is the case, developers may
start moaning with the infamous "You said that would be available"

I do believe however that features seriously being considered for
implementation would actually be a very good thing to advertise as it
could act as a bit of a pre-sales pitch to potential users instead of
the need to investigate a release to find out whether or not it is worth
investing in.

Anyway, as everyone is firing suggestions at the reflector at the
moment, I thought I would take the opportunity to give my input ...

  1. Undo  -  A feature that is far overdue !
  2. More of a 'Windows' feel including the double-click and
triple-click features to select text
  3. Multi-select on panel view allowing multiple drags, property
changes etc...
  4. A similar feature to a 'Frame' in VB allowing a series of objects
to be grouped
  5. 'LOCK FILE' and 'UNLOCK FILE' commands in the TO FILE and FROM
FILE objects for secure multi-user file access.

Suggestion 5 was made officially in the days leading up to the release
of Vee 4.0 but as yet, I have received no feedback as to when a facility
such as this would be available.

Anyway, enough from me.

Regards,

James

-------------------------------------------------------
James Atkin BEng(Hons) MIEE
Software Engineer
Mitec Telecom Ltd
The Arenson Centre
Arenson Way
Dunstable, Bedfordshire
LU5 5UL
Phone : +44 (0) 1582 445075
-------------------------------------------------------

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes