AnsweredAssumed Answered

vrf AW: USB-GPIB Interface 82357A

Question asked by d.sperling on Oct 25, 2002
Hello Wolfgang,

the Logical Adress Setup is in the IO Library Control.
Select the GPIB Interface and set the device to Logical Unit 14.
When it not work then you have an NI card still configured in your system.

Best regards

Dietmar

---

Hello
has everyboby experience with the USB-GPIB Interface 82357A.
I like to set the logical address from 7 (default Agilent) to 14 (default
NI).


Mit freundlichen Grssen

Wolfgang Ruckert
Astrium GmbH
88039 Friedrichshafen
Tel  (0) 7545 84920
Fax (0) 7545 8184920


-


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes