AnsweredAssumed Answered

vrf ProcessView.vee

Question asked by VRFuser on Jul 31, 2003
I've fixed up a few old problems with this thing. Those of you who wish to
get an updated copy please email me. Bug fixes follow:

  1) Removed bitmap paths.

  2) Fixed "OS Dependent" in LoadLibs. Toolhelp functions are imported
     from kernel32.dll for NT versions >= 5 and from toolhelp.dll for
     all other Windows versions. The whichOS function is not used anymore.

  3) Fixed GetFileData. Because I was reading file data as Int32, VEE
     would not read files who's sizes were not divisible by 4. Sometimes
     when you double-click on a "File Header" node nothing would happen.
     This is now fixed.

  4) Cleaned up several of the bit to string decoding functions so
     they're less stupid. I have no idea what I was thinking.
-SHAWN-


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes