AnsweredAssumed Answered

vrf Date: Tue, 23 Jul 2002 17:02:04 -0400

Question asked by VRFuser on Jul 23, 2002

Hi Mike,

The result in both are OK (using VEE 6.01) in the alphanumeric object. However, the translation from real to integer is done at the input pin in the UserObject itself and it is done before arriving to alphanumeric object in UserFunction (If you enable the show terminals in the alphanumeric you can see it).

I suspect it is due to an UO is called only in one place in the application but a UF can be called several times in different places.

Regards,



-----Mensaje original-----
De: owner-vrf@lvld.agilent.com [mailto:owner-vrf@lvld.agilent.com]En
nombre de Mike Groves
Enviado el: martes, 23 de julio de 2002 22:51
Para: VEE Reflector (E-mail)
Asunto: Function Bug??


My original post was to reveal a possible bug in VEE.
Folow the attachment to see what I mean...

Mike Groves
Cree Microwave
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes