AnsweredAssumed Answered

vrf Integrating graphical buttons with images

Question asked by jcmartin on Nov 24, 2004

We are using an ActiveX of Iocomp (http://www.iocomp.com/) in order to show a RF matix. Specifically the LedMatrix. You can download and test it.

Regards



> -----Mensaje original-----
> De: MALPHURS,STEVE (A-Sonoma,ex1) [mailto:steve_malphurs@agilent.com]
> Enviado el: mircoles, 24 de noviembre de 2004 22:04
> Para: VRF
> Asunto: [vrf] Integrating graphical buttons with images
>
>
> Hello VRF,
>
> I am creating a control panel for a RF switch matrix. I want
> to show the block diagram of the matrix and then be able to
> click on the graphic image of the individual switch to change
> the switch setting. I can create the buttons that have the
> two images for the open and closed switch positions, but the
> problem is integrating these buttons with the rest of the
> block diagram image. The best I can do is set the background
> image of a panel with my block diagram and then place the
> buttons in their correct positions, however, the lines do not
> quite line up. Does anyone have any suggestions on how this
> might be done?
>
> Regards,
> Steve Malphurs
>
>
> ---
> You are currently subscribed to vrf as: jcmartin@indra.es
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@agilent.com". 
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".
>

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes