AnsweredAssumed Answered

vrf runtime setup of Default preferences

Question asked by VRFuser on Jul 14, 2003
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 5.50.4807.2300" name=GENERATOR></HEAD><BODY><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>Hi All</FONT></SPAN></DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2></FONT></SPAN> </DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>Does anybody know if it is possible to setup the default settings of vee, runtime from a program? </FONT></SPAN></DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2></FONT></SPAN> </DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>I have a calibration program for a test system and because of the wanted accuracy, we want to switch the default "real" value to "Scientific" with 8 fractional digits (yes we have seen rounding errors if we use a lesser value).</FONT></SPAN></DIV><DIV><SPAN class=923141811-15072003></SPAN> </DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>Right now, I'm using a big pop-up box telling the operator to check the settings, but if it could be set runtime it would be a much smoother solution.</FONT></SPAN></DIV><DIV><SPAN class=923141811-15072003></SPAN> </DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>Best Regards</FONT></SPAN></DIV><DIV><SPAN class=923141811-15072003></SPAN> </DIV><DIV><SPAN class=923141811-15072003><FONT face=Arial size=2>Martin</FONT> </SPAN></DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>  

Outcomes