<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 3.2//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=us-ascii"><META NAME="Generator" CONTENT="MS Exchange Server version 6.0.6493.0"><TITLE>Error number 400 Value A is nil or empty (could be zero-element array)</TITLE></HEAD><BODY><!-- Converted from text/rtf format --><P><FONT SIZE=2 FACE="Arial">Hello VRFers,</FONT></P><P> <FONT SIZE=2 FACE="Arial">I was running VEE 3.0 on a UNIX platform on a vintage HP 382. My task is to convert all existing VEE programs to a PC platform. I am using VEE 6.2 but I am running it in the VEE 3.0 mode. On the UNIX platform everything works fine. I have a "to string location" which essentially feeds data to one input of a collector. The other input to the collector is the XEQ. The output of the collector is input "A" to the formula box. The formula for the formula box is "OutputString+A(B)". Input "b" to the formula box is just a number of the array that is being passed through. Whenever my data is 1111's or 11111's 00000's and XXXXX's everything works fine, however, when I run a string of XXXXXXX's or all 0000000's I get error 400 on the PC platform.</FONT></P><P> <FONT SIZE=2 FACE="Arial">Does anyone know why this happens? Is there a fix out there? Can I turn off this error checking (IE let the data flow as it used to in the older version?)</FONT></P><P> <FONT SIZE=2 FACE="Arial">Any suggestions will be greatly appreciated.</FONT></P><P><FONT COLOR="#0000FF" SIZE=5 FACE="Script">Larry A. Cote'</FONT><BR><FONT SIZE=2 FACE="Arial">Test Methods Engineer</FONT><BR><FONT SIZE=2 FACE="Arial">Lockheed Martin Maritime Systems & Sensors</FONT><BR><FONT SIZE=2 FACE="Arial">E-mail:</FONT> <FONT COLOR="#800080" SIZE=2 FACE="Courier New">larry.a.cote@lmco.com</FONT><BR><FONT SIZE=2 FACE="Arial">Phone 856-722-3945</FONT><BR><FONT SIZE=2 FACE="Arial">Fax 856-722-7768</FONT></P><BR>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>