AnsweredAssumed Answered

vrf Vee 7 Features

Question asked by VRFuser on Mar 4, 2004
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2800.1276" name=GENERATOR></HEAD><BODY><DIV><SPAN class=041122720-05032004><FONT face=Arial size=2>Scott (Bayes),</FONT></SPAN></DIV><DIV><SPAN class=041122720-05032004><FONT face=Arial size=2></FONT></SPAN> </DIV><DIV><SPAN class=041122720-05032004><FONT face=Arial size=2>Although it is deemed poor programming practice to allow any one object or function to occupy more space than can be seen on one screen without scrolling (something which I have NEVER EVER done), do you have any idea if there will be a zoom function in detail view.  This would greatly help to debug/clean up those nightmare programs that have detail views the size of a small county.  Also, what about a "group select/move/size" in panel view?  I remember hearing that properties will be batch editable.</FONT></SPAN></DIV><DIV><SPAN class=041122720-05032004><FONT face=Arial size=2></FONT></SPAN> </DIV><DIV><SPAN class=041122720-05032004><FONT face=Arial size=2></FONT></SPAN> </DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>  

Outcomes