AnsweredAssumed Answered

vrf controlling pop-up dialog box via panel view?

Question asked by bill.ossmann on Nov 13, 2003

Enrique,

The following from the VEE help:

The default location of the pop-up dialog box is approximately at the center of the work area. If you move it, next time it will pop-up to the new location.
.
.
.
The pop-up dialog box and the error dialog box are only displayed while the program is running. While the pop-up dialog box is displayed, the entire program pauses execution, then continues when the dialog box is closed.

In other words, I don't think you can specify where the dialog shows up except by moving it there while the program is running, which also means the user can move it around. You can place the dialog box object on the panel, but that won't actually do
anything useful. If you really need to control the physical configuration of inputs on the screen, use panels.

Regards,
--
Bill Ossmann
Philips Ultrasound
e-mail:  bill.ossmann@philips.com




hi bill,

i'm trying to place the "data ->dialog box ->text input" display to
pop/appear on the panel area, if this is possible?

thanks,
Enrique "IKE" Velasco, Jr.
Junior Engineer


Delta Energy Systems (Arizona), Inc.
4400 E. Broadway Blvd., Suite 803, Tucson, AZ, 85715, USA
T +1 520 326 8401, F +1 520 326 8366
M +1 520 370 4537
enrique.velasco@delta-es.com
www.deltaenergysystems.com







                    bill.ossmann@p
                    hilips.com            To:     VRF <vrf@agilent.com>
                                          cc:
                    11/14/2003            Subject:     [vrf] Re: controlling pop-up dialog box via panel view?
                    11:18 AM
                    Please respond
                    to
                    bill.ossmann






Enrique,

I am not sure whether you want to use a panel as a dialog box, or to have a
dialog box pop up from a panel. This will do both.
Try entering "Manual Fc (MHz)" < 0 or "Manual Fc (MHz)" > 100 to see a
pop-up panel.


--
Bill Ossmann
Philips Ultrasound
e-mail:  bill.ossmann@philips.com

(See attached file: PanelDialog.vee)




                                                   To:   VRF
<vrf@agilent.com>
                                                   cc:   (bcc: Bill
Ossmann/ANR/MS/PHILIPS)
                                                   Subject:    [vrf]
controlling pop-up dialog box via panel view?

               "Enrique Velasco"                   Classification:

               <Enrique.Velasco@ascom.c

               om>


               11/14/2003 11:57

               Please respond to

               "Enrique Velasco"







hello all,

does anyone of you have an example on how to control pop-up dialog boxes to
appear or show through the panel view?

thank you in advance...

Enrique "IKE" Velasco, Jr.
Junior Engineer


Delta Energy Systems (Arizona), Inc.
4400 E. Broadway Blvd., Suite 803, Tucson, AZ, 85715, USA
T +1 520 326 8401, F +1 520 326 8366
M +1 520 370 4537
enrique.velasco@delta-es.com
www.deltaenergysystems.com






---
You are currently subscribed to vrf as: bill.ossmann@philips.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".



(See attached file: PanelDialog.vee)---
You are currently subscribed to vrf as: Enrique.Velasco@ascom.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".


---
You are currently subscribed to vrf as: bill.ossmann@philips.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".







---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes