AnsweredAssumed Answered

vrf AW: Printout.

Question asked by VRFuser on Aug 22, 2002
Hello,

I used a x vs. y-plot and put comments and some informations in the title of
the plot window using a control input.
After the measurement finishes one right-mouse click, select plot and the
print out starts.
I also implemented a "print screen" object (located under the I/O menu) to
print out things with more comments (which can not be fitted to one line).
Best regards,

Martin Alles

> -----Ursprngliche Nachricht-----
> Von:     Andy.Cole@raytheon.co.uk [SMTP:Andy.Cole@raytheon.co.uk]
> Gesendet am:     Freitag, 23. August 2002 13:30
> An:     VEE vrf
> Betreff:     [vrf] Printout.
> Wichtigkeit:     Hoch
>
> Ideas?
>
> Shawn tried to help a while ago when I was trying to communicate with
> Excel
> from Vee. However, I have since discovered that out IT department has
> switched off all the Active X controls in our PC's and will not allow us
> to
> put them back on. Therefore I'm stuck with trying to get my info onto a
> printer with Vee alone.
>
> I am trying to get a printout of the displayed plot from an XY Plot
> object,
> together with some text information held in several variables, on to the
> same piece of paper. Short of having several pop up functions and then
> doing a screen dump I'm a bit short of ideas.
>
> Incidentally, this is Vee 5 and I have a Epson 880 sitting at the end of
> the network.
> Any thoughts???
>
> Regards,
>
> Andy Cole.
> Raytheon Systems Ltd.
>
>
> ---
> You are currently subscribed to vrf as: Martin.Alles@hno.atmel.com
> To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email
> "vrf@it.lists.it.agilent.com". 
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@it.lists.it.agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes