AnsweredAssumed Answered

vrf Red Death in China

Question asked by VRFuser on Dec 10, 2003
> "Internal Error Connect () failed error = 10065".

Error 10065 = A socket operation was attempted to an unreachable host.

The Box Of The Red Death seems a bit extreme though. Don't know why that is.
I suppose localization issues may be responsible, though it's difficult to
understand how. If the red info indicates the socket caused the error, then
I would think it's a combination MS / VEE problem: as far as I know, VEE is
not UNICODE aware, but if it's running on Chinese Windows this could be a
problem when passing strings retrieved from strictly MBCS resources, i.e.
the socket error string.
-SHAWN-


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes