AnsweredAssumed Answered

vrf VEE via LAN

Question asked by PacoLopez on Nov 24, 2003
Hi Hans-Joachim,

What you need is already available, at least, if you can control your
instruments thru HPIB, of course. It's called HPIB gateway and Agilent has 2
models (E5810A and E2050A/B,obsoleted right now). You only need a lan
connection and minor changes in your application to replace the old HPIB
connections to a lan controled connection. Have you notice the Gateway entry
field in the intrument properties???

Hope it helps,

Paco

-----Original Message-----
From: VEE user at ESF GmbH [mailto:vee@esf-gmbh.de]
Sent: Tuesday, November 25, 2003 11:05 AM
To: VRF
Subject: [vrf] VEE via LAN


Dear all,


a big VEE program is in operation since a couple of months. It runs quite
stable locally in a RF chamber. Now I need to control the instruments
remotely via a LAN. I tried to understand the LAN functionality of VEE
reading the manual. This did not really help me in short time.

Is there a "simple" possibility to implement remote control of the
instruments via LAN without touching major parts of the existing VEE
program. I would like to have just a switch that tells to the computer in
the RF chamber "take all commands from remote computer at x.x.x.x". The
remote computer should be advised "send all commands to remote computer
y.y.y.y where the GPIB instruments are connected"

Is this just a dream or is this possible? Are there guidelines how to
achieve it available?

Actually in the final end the remote control has to be via internet.


Sincerely
Hans-Joachim Fischer




------------------------------------------
ESF GmbH
Brennerweg 7
D-89143 Blaubeuren
+49-7344-919693
+49-7344-919691 (fax)
+49-175-40 74 5 74 (GSM)
http://www.esf-gmbh.de
------------------------------------------


---
You are currently subscribed to vrf as: paco.lopez@hp.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes