AnsweredAssumed Answered

vrf NI DAQ I/O Card

Question asked by tapio.ronkainen on Jan 19, 2004
?

Do you mean Computerboard's DIO 24 board (sounds like one)? For that I suggest that you get the I/O lib from computerboards, that solves all problems (works even with XP and W2k).

BR, Tapio

> -----Original Message-----
> From: ext d b [mailto:dd_besgrove@hotmail.com]
> Sent: 19 January, 2004 22:59
> To: VRF
> Subject: [vrf] NI DAQ I/O Card
>
>
> Chaps,
> Many thanks for the replies on WAV files. They were very
> useful. I have
> another problem. I want to talk to a National Instruments DAQ
> PCMCIA Card
> DIO 24. This card is used to set a number of lines high or
> low for switching
> external circuitary. My OS recognizes the card is in the
> system, but VEE I/O
> Config utility cannot find it. Is the because the utility can
> only recognize
> GPIB, serial and VXI kit ?
> How do I talk to the DIO card using VEE ? I have all the NI
> documentation.
> Do I really need to program in register level ? Is there a
> DLL that is
> required ? Does anyone have any examples ?
> Really appreciate any help,
> Thanks,
> Dan Besgrove
>
> _________________________________________________________________
> Stay in touch with absent friends - get MSN Messenger
> http://www.msn.co.uk/messenger
>
>
> ---
> You are currently subscribed to vrf as: tapio.ronkainen@nokia.com
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@agilent.com". 
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".
> Send your favorite VEE example to "VRF-EXAMPLES@agilent.com"
> for possible inclusion in VEE 7.0!
>

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Send your favorite VEE example to "VRF-EXAMPLES@agilent.com" for possible inclusion in VEE 7.0!

Outcomes