AnsweredAssumed Answered

vrf Serial interface error...

Question asked by VRFuser on Jul 9, 2001
I've also received this error upon switching programs that previously ran fine under VEE 5 to VEE 6, and I have no explanation for it.  For myself, when the error is cleared, it usually works fine.  I'm beginning to suspect a bug in VEE 6...


Reiner Schlieker
Test Equipment Designer
Siemens Milltronics Process Instruments Inc.
Phone: (705) 740-7553
Fax:      (705) 740-7692
e-mail: reiners@milltronics.com


>>> "Rudrow, Doug" <Doug_Rudrow@spectrian.com> 07/09/01 02:09PM >>>

     I'm using VEE 6.0 to communicate with one of our products over a
serial interface. When I run the program I get an error when I try to send a
command to the unit. The error reads: IO error or timeout occurred SICL call
made with bad parameter. Unable to set receive buffer size of 4096 bytes.
This only happens after I've clicked the main run button, if I send the
command using a "Start" object from within the program it works fine. Anyone
run into this before?

Doug Rudrow
R&D Test Engineer
Spectrian Inc.

P.S. - I've tried changing the buffer size and the timeout length.

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes