AnsweredAssumed Answered

vrf VEE via LAN (more on Remote Desktop)

Question asked by daras Employee on Dec 2, 2003
Hello Hans,

Is my assumption correct that your existing VEE program controls your instruments, using GPIB?  And that in your new setup you have a distance limitations that make it difficult or impossible to use GPIB cables?  If this is the case and you want to use LAN to communicate with your instruments and not change any of your VEE code, your best option is to use a LAN-TO-GPIB gateway (both Agilent and National Instruments make this box).  The gateway has a GPIB and a LAN port.  You put it near your instruments and connect them to its GPIB port.  You then connect the gateway to the same LAN as your controller (the PC that is running your VEE program).  You setup the gateway with a LAN address and a hostname and in your VEE program you go to your instrument IO setup and in the property of each of the GPIB configured devices, you change the value of the Gateway from "This Host" to the host name of the your gateway.  I haven't checked the price of a gateway recently, but it can't be more than a few hundred dollars and if you really have a large program that is complex and difficult to change, this is the most efficient and cost effective way of solving this problem.

Hope this helps,

Dara Sariaslani
Agilent Technologies

-----Original Message-----
From: VEE user at ESF GmbH [mailto:vee@esf-gmbh.de]
Sent: Wednesday, November 26, 2003 12:33 AM
Subject: AW: RE: VEE via LAN (more on Remote Desktop)


Dear all,


thank you for your suggestions.
Definitively I will not use XP!
What I need is a mechanisme inside VEE.
Unfortunately the manual is not very precise with respect to LAN functionality. I will now start to evaluate the various proposals.


Sincerely
Hans-Joachim

-----Ursprngliche Nachricht-----
Von: REED,KIRK (A-LittleFalls,ex1) [mailto:kirk_reed@agilent.com]
Gesendet: Dienstag, 25. November 2003 19:09
An: VRF
Betreff: [vrf] RE: VEE via LAN (more on Remote Desktop)


Richard touched on the Remote Desktop.  This is the way to go.  Mike thought both computers needed to be Windows XP.  Not so, Microsoft has released the programs to have any windows 95 and later pc control a Windows XP Pro. Windows Home is only capable of Remote Assistance, where Pro goes one step further to with Remote Desktop.  It used to be only available for Windows servers, and then XP Pro added the capability.



We use all our pcs to control XP Pro machines.  I use it even to control work pcs in China, California, or just at work.  It is as if you were sitting in front of the computer.  If Hans's computer in the RF chamber is XP Pro, he just needs to "allow" remote control of the pc through Remote Desktop.  Enable this by going to System Properties, and on the Remote tab enabling it.



See the Microsoft website that describes it in detail, and gives links for the client side software to access the Windows XP Pro machine (host).



http://www.microsoft.com/windowsxp/pro/using/howto/gomobile/remotedesktop/de
fault.asp



I use RealVNC, Remote Desktop, and Remote Assistance.  I only use RealVNC when controlling a NON XP machine.  Remote Assistance allows two people to share the same pc, Remote Desktop locks the screen on the host.



One nice thing is it resizes the host computer screen info to the client's resolution, so unlike VNC, you are not moving the scroll bars all around to view all the host's info.  It even redirects your printer info to the client's printer.  Not sure about Vee though, since you can setup printer info in preferences.  I don't use printers much with Vee remotely.



Hans, this will solve your problems real fast, IF your RF chamber machine is XP Pro.  This is one nice freebie Microsoft has given us, and it works GREAT!





-----Original Message-----

From: Mike Groves [mailto:mikegroves@pacbell.net]

Sent: Tuesday, November 25, 2003 6:25 AM

To: VRF

Subject: [vrf] RE: VEE via LAN



You didn't mention what platform the VEE programs were running on, but

I would think the absolute easiest way to do this, without touching your

VEE code, would be to use one of the many remote control programs that

are available. Here are my suggestions...



1) If all of the machines are running Windows XP, you can use the "Remote

Desktop Connection" built into XP to get one PC to control another.



2) If all the PC's involved are running Windows, it doesn't get much easier

than using pcAnywhere from Symantec. Version 11 is outstanding. It will cost

a little bit, but I've used this for years to control VEE machines remotely

and it does an excellent job.

http://enterprisesecurity.symantec.com/products/products.cfm?ProductID=2



3) If these are not all Windows machines, or you would like to get by very

inexpensively, then you can go with RealVNC. (www.realvnc.com/winvnc.html)

I used it years ago. It has the advantage of remote controlling dissimilar

machines and best of all, it's free!



My suggestion is to leave your VEE code as is and install one of these.



Cheers!

Mike Groves



-----Original Message-----

From: VEE user at ESF GmbH [mailto:vee@esf-gmbh.de]

Sent: Tuesday, November 25, 2003 2:05 AM

To: VRF

Subject: [vrf] VEE via LAN





Dear all,





a big VEE program is in operation since a couple of months. It runs quite

stable locally in a RF chamber. Now I need to control the instruments

remotely via a LAN. I tried to understand the LAN functionality of VEE

reading the manual. This did not really help me in short time.



Is there a "simple" possibility to implement remote control of the

instruments via LAN without touching major parts of the existing VEE

program. I would like to have just a switch that tells to the computer in

the RF chamber "take all commands from remote computer at x.x.x.x". The

remote computer should be advised "send all commands to remote computer

y.y.y.y where the GPIB instruments are connected"



Is this just a dream or is this possible? Are there guidelines how to

achieve it available?



Actually in the final end the remote control has to be via internet.





Sincerely

Hans-Joachim Fischer









------------------------------------------

ESF GmbH

Brennerweg 7

D-89143 Blaubeuren

+49-7344-919693

+49-7344-919691 (fax)

+49-175-40 74 5 74 (GSM)

http://www.esf-gmbh.de

------------------------------------------





---

You are currently subscribed to vrf as: mikegroves@pacbell.net

To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".

To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".

To send messages to this mailing list,  email "vrf@agilent.com".

If you need help with the mailing list send a message to

"owner-vrf@it.lists.it.agilent.com".





---

You are currently subscribed to vrf as: kirk_reed@agilent.com

To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".

To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".

To send messages to this mailing list,  email "vrf@agilent.com".

If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".




  _____

<< ella for Spam Control >> has removed 812 Spam messages and set aside 26 Read Later for me You can use it too - and it's FREE!  www.ellaforspam.com <http://www.ellaforspam.com>

---
You are currently subscribed to vrf as: vee@esf-gmbh.de
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes