AnsweredAssumed Answered

vrf RS232 HPUXvs PC

Question asked by VRFuser on Sep 30, 2001
Hi Stan,

* On Fri, Sep 28, 2001 at 03:35:40PM -0700, Stan Bischof wrote:
> I am seeing several symptoms but the two strangest are
> ...
> I have verified all settings that I can think of- and basic comm
> works but is flaky as outlined above.

That really sounds difficult to track.
Does it make a difference if you disable all that FIFO settings
in windows (settings of the according com port)?
Does it make a differenz if you increase or decrease the
buffer sizes?
Is that behavior somehow dependent of the used baud rate?

If nothing helps I think you would have to use an oszilloskope
to watch the activity of the ports...

Rgds.
Heiko.

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes