AnsweredAssumed Answered

PLTS - Automatic Fixture Removal

Question asked by Lumberjack on Mar 20, 2012
Latest reply on Mar 21, 2012 by Lumberjack
I am running a bunch of thru files through the "automatic fixture removal" utilitie in PLTS, and saving out the de-embeded fixture files.  It works just fine on most of the files.  On others I am getting an error stating "the length of the source freq. and data are not identical, export can not be achieved".  The s2p files seem fine as far as I can tell.

To be more specific I am importing the attached thru file.  Then using the automatic fixture removal and loading the same thru file to get the de-embeded fixture files (1 and 2), and writing them out.  Now if I uncheck the "Output De-embeded Fixture Files" the utilitie seems to work just fine.  The graph looks as expected.  I only get the error when trying to write the files out.

The version of PLTS is 5.500.  I have also attached one of the s2p files for your convenience.

Any help would be greatly appreciated, thanks.  

Outcomes