AnsweredAssumed Answered

vrf Changing COM settings

Question asked by VRFuser on Feb 3, 2004
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><TITLE>Changing COM settings</TITLE><META content="MSHTML 6.00.2800.1276" name=GENERATOR></HEAD><BODY><DIV><FONT face=Arial color=#0000ff size=2><SPAN class=494215119-03022004>I do it without any problem.  I have defined 2 instruments in the instrument manager: one at lower speed and the other at higher speed.  When I change from one "instrument" to the other, I sent a "execute reset" first (optionnally followed by a "execute close").</SPAN></FONT></DIV><BLOCKQUOTE>  <DIV><FONT face="Times New Roman" size=2>-----Message   d'origine-----<BR><B>De:</B> Ross Bledsoe   [mailto:RBLEDSOE@Coinco.com]<BR><B>Date:</B> 3 fvrier 2004   14:46<BR><BR></FONT></DIV>  <P><FONT face=Arial>I have an VEE application that requires changing the com   port settings on the fly.  For example I need to send data at 9600 bps, 8   data bits, odd parity, and 1 stop bit.  I then need to send data out the   same com port at 9600 bps, 8 data bits, even parity and 2 stop bits.</FONT></P>  <P><FONT face=Arial>Can I change these port settings in the middle of the   application ?</FONT> <BR><FONT face=Arial>Thanks in advance</FONT> </P></BLOCKQUOTE>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".<BR>Send your favorite VEE example to "VRF-EXAMPLES@agilent.com" for possible inclusion in VEE 7.0!</BODY></HTML>  

Outcomes