AnsweredAssumed Answered

vrf Temperatura sensor

Question asked by pbortot on Mar 25, 2004
Hi list,
before i go too deep into details, just the simple question- Is VEE slower
than LAbview if you use an IO-Card ?
We do have an old IO-Card which is called via .dll
The test data access via VEE gets about 100 Values , via Visual BAsic and
Labview about 1000.
Is VEE in principle slower than the others in that case ?
Otherwise i can go in more detail ...-
It on a 500 MHz machine.

Thanks for help,.
detlef

This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.

Visit our internet site at http://www.pilkington.com

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes