> I'll second that! (Recursion)
Me too.
> Recursion is hardly ever needed
Oh i dunno! Once you start thinking in terms of recursive algorithms you
start seeing them everywhere.
> I needed to check the size of each sub folder in a folder
> once. I needed to use a VB DLL to do this using recursion.
> P.I.T.A.
Totally. There is somewhat of a workaround. If you have the Script control
installed you can write recursion in VBS or JScript. It's still no fun
though - just adding the code to a script control instance gets messy.
> Also the need for callback functions.
A great need for Windows interaction. Unfortunately since VEE isn't compiled
there will never be an executable address of anything, but you can kind of
do it. Use the address of a function in an Automation library as the
callback address. Have the library callback function fire an event, and
catch the event with VEE. Not quite the same, but it works.
-SHAWN-
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Me too.
> Recursion is hardly ever needed
Oh i dunno! Once you start thinking in terms of recursive algorithms you
start seeing them everywhere.
> I needed to check the size of each sub folder in a folder
> once. I needed to use a VB DLL to do this using recursion.
> P.I.T.A.
Totally. There is somewhat of a workaround. If you have the Script control
installed you can write recursion in VBS or JScript. It's still no fun
though - just adding the code to a script control instance gets messy.
> Also the need for callback functions.
A great need for Windows interaction. Unfortunately since VEE isn't compiled
there will never be an executable address of anything, but you can kind of
do it. Use the address of a function in an Automation library as the
callback address. Have the library callback function fire an event, and
catch the event with VEE. Not quite the same, but it works.
-SHAWN-
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Sorry about making trouble to yourselves.
I added publication numbers (****-***EN) and its URLs to the list.
Please take a look.
(Application Note 1465-8, pub. no. 5988-9823EN $B!K (B
$B!H (BTest-System Development Guide $B!' (BOperational Maintenance $B!I (B
http://cp.literature.agilent.com/litweb/pdf/5988-9823EN.pdf
(Application Note 1465-7, pub. no. 5988-9822EN $B!K (B
$B!H (BTest-System Development Guide $B!' (BMaximizing System Throughput
and Optimizing System Deployment $B!I (B!!
http://cp.literature.agilent.com/litweb/pdf/5988-9822EN.pdf
(Application Note 1465-4, pub. no. 5988-9819EN)
$B!H (BTest-System Development Guide $B!' (BChoosing Your
Test-System Software Architecture $B!I (B!!
Sorry! URL Not Found.
(Application Note 1465-3, pub. no. 5989-0123EN)
$B!H (BTest-System Development Guide $B!' (BUnderstanding
Drivers and Direct I/O $B!I (B
or
(Application Note 1475-1)
"Modern Connectivity - Using USB and LAN I/O Converters"
http://cp.literature.agilent.com/litweb/pdf/5989-0123EN.pdf
(Application Note 1465-2, pub. no. 5988-9818EN)
$B!H (BTest-System Development Guide $B!' (BComputer I/O Considerations $B!I (B
http://cp.literature.agilent.com/litweb/pdf/5988-9818EN.pdf
(Application Note 1465-1, pub. no. 5988-9747EN)
$B!H (BTest-System Development Guide $B!' (BIntroduction to Test-System Design $B!I (B!!
http://cp.literature.agilent.com/litweb/pdf/5988-9747EN.pdf
Regards,
FUKUI Yutaka
M.Kozlov@ifw-dresden.de wrote:
>
> Hi FUKUI Yutaka,
>
> Would you, please, define more exactly the reference on these Application
> Notes. When I try to find these Application Notes I get only
>
> Test-System
> Development Guide
> Understanding Drivers and Direct I/O
> Application Note 1465-3
>
> Thanks in advance.
>
> Mikhail Kozlov
>
--
*****************************************************************
* $BJ!0f!!K-!J (BFUKUI Yutaka)
* E-Mail: fukui.yutaka@jp.fujitsu.com
* $BIY;NDL3t<02q<R!!@n:j9)>l (B
* $B$b$N$E$/$j?d?JKIt!&@8;:5;=Q3+H/E}3gIt!K7WB,@_Hw3+H/It (B
* $B7WB,@_Hw3+H/It (BHomePage http://www.psl.fujitsu.co.jp/htd2/ksk/
* $B@n:j;TCf866h>e>.EDCf#4 (B- $B#1 (B- $B#1!!M9JXHV9f!' (B211-8588
* TEL $B!!30@~ (B 044-754-3657, $B!!Fb@~ (B 711-3-1966,7
* FAX $B!!30@~ (B 044-754-3509, $B!!Fb@~ (B 711-3-5359
*****************************************************************
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".