<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 5.50.4937.800" name=GENERATOR></HEAD><BODY><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>Hi VRF'ers</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>I want to show a custom picture on a toggle control for ON and OFF. This is no problem, as it is possible to select which picture to use.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>But the problem is, that the link to the picture is static. Which means that if the users of my application choose to install the program in an other library than I had in mind, the pictures don't show.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>Does anybody have an idea on how to make a dynamic link to the picture on a toggle control?</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>Best regards</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=517372509-19042004>Martin</SPAN></FONT></DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
A command would look like this ":CFG 1,11".
I want to include a note on the same line indicating what the configuration does.
In other words, I want the direct IO box transaction to look something like ":CFG 1,11" Changes instrument to auto range mode.
Is there a key sequence to tell VEE to ignore anything after the ":CFG 1,11"?
Thanks,
Jon Griggs
mailto:jgriggs@crownintl.com
Test Engineer
Crown International
1718 West Mishawaka Road
Elkhart, IN 46517
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".