<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 3.2//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META NAME="Generator" CONTENT="MS Exchange Server version 5.5.2654.45"><TITLE>RE: [vrf] Re: Streaming Serial Data Capture</TITLE></HEAD><BODY><P><FONT SIZE=2>Greg:</FONT><BR><FONT SIZE=2>> Are you sure your company firewall isn't grabbing the attachment?</FONT><BR><FONT SIZE=2>> Or whatever your using to read your mail?</FONT></P><P><FONT SIZE=2>The hlp files are stripped here directly from exchange server.</FONT><BR><FONT SIZE=2>This is a rule that was set for the anti-virus.</FONT></P><P><FONT SIZE=2>Shawn:</FONT><BR><FONT SIZE=2>> NO WAY! Good god - this insanity must end! I know .hlp files can contain</FONT><BR><FONT SIZE=2>> macros, but geez louise - they can't do any damage.</FONT></P><P><FONT SIZE=2>I can't argue with you...</FONT></P><BR><P><FONT SIZE=2>-----Message d'origine-----</FONT><BR><FONT SIZE=2>De: Shawn Fessenden [<A HREF="mailto:shawn@testech-ltd.com">mailto:shawn@testech-ltd.com</A>]</FONT><BR><FONT SIZE=2>Date: 7 mai 2004 01:57</FONT></P><P><FONT SIZE=2>> the .HLP file was collected by Outlook because</FONT><BR><FONT SIZE=2>> it thought that was a potentially unsafe file.</FONT></P><P><FONT SIZE=2>NO WAY! Good god - this insanity must end! I know .hlp files can contain</FONT><BR><FONT SIZE=2>macros, but geez louise - they can't do any damage.</FONT></P><P><FONT SIZE=2>Ok, I'm officially placing an item on my "Things To Do Real Soon Now"</FONT><BR><FONT SIZE=2>agenda: find a way around all this crazy Outlook carpola. Even if it has to</FONT><BR><FONT SIZE=2>be a blessed binary patch then so be it. This has gone way, WAY too far.</FONT></P><P><FONT SIZE=2>In the mean time (because RSN never seems to come), for all of those out</FONT><BR><FONT SIZE=2>there who use Outlook to have VEE email reports and notifications to you, I</FONT><BR><FONT SIZE=2>found a nifty little utility to get around that annoying "Another program is</FONT><BR><FONT SIZE=2>trying to send mail..." warning. It's called Express ClickYes and it's free.</FONT><BR><FONT SIZE=2>It can be found at:</FONT></P><P><FONT SIZE=2><A HREF="http://www.express-soft.com/mailmate/clickyes.html" TARGET="_blank">http://www.express-soft.com/mailmate/clickyes.html</A></FONT></P><P><FONT SIZE=2>Way to go Express Soft. I will be including ECY support in everything I do</FONT><BR><FONT SIZE=2>with mail from now on.</FONT></P><BR><P><FONT SIZE=2>-----Message d'origine-----</FONT><BR><FONT SIZE=2>De: Gregg C Levine [<A HREF="mailto:hansolofalcon@worldnet.att.net">mailto:hansolofalcon@worldnet.att.net</A>]</FONT><BR><FONT SIZE=2>Date: 6 mai 2004 15:55</FONT></P><P><FONT SIZE=2>Are you sure your company firewall isn't grabbing the attachment? Or</FONT><BR><FONT SIZE=2>whatever your using to read your mail? As it happens with me, I</FONT><BR><FONT SIZE=2>received all versions, the .HLP file was collected by Outlook because</FONT><BR><FONT SIZE=2>it thought that was a potentially unsafe file. It wasn't but I suspect</FONT><BR><FONT SIZE=2>that was an example of Microsoft stupidity at work. </FONT></P><BR><P><FONT SIZE=2>-----Original Message-----</FONT><BR><FONT SIZE=2>From: Beliveau, Bruno [<A HREF="mailto:BrunoBeliveau@solectron.com">mailto:BrunoBeliveau@solectron.com</A>] </FONT><BR><FONT SIZE=2>Sent: Thursday, May 06, 2004 8:34 AM</FONT></P><P><FONT SIZE=2>In both versions here, the file SERCOMM.HLP was stripped. The rest</FONT><BR><FONT SIZE=2>came thru OK. </FONT></P><BR><P><FONT SIZE=2>-----Message d'origine----- </FONT><BR><FONT SIZE=2>De: Analysetechnik@t-online.de [<A HREF="mailto:Analysetechnik@t-online.de">mailto:Analysetechnik@t-online.de</A>] </FONT><BR><FONT SIZE=2>Date: 6 mai 2004 08:11 </FONT></P><P><FONT SIZE=2>here it is! </FONT><BR><FONT SIZE=2>Because some servers block *.zip and others *.vee files I'll send</FONT><BR><FONT SIZE=2>both </FONT><BR><FONT SIZE=2>versions. </FONT></P>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
Hi VRF,
I am trying to capture alpha numeric data that is streaming into a serial
port on my PC. I would like to capture this data between known starting
and ending points, then grab specific information contained within the
capture. I can do this by running Hyperterminal as a PC Execute within
Vee...Writing the Hyperterminal Data to a txt file of the HDD...Then
reading the text file back into VEE...but it seems like the hard way to do
it. Is there an easier way to get this information into VEE? The data
that I am capturing is listed below in bold and repeats continuously,
although I only need to capture one pass of information.
I am using VEE 7.0 on an XP machine.
EnabPort 1 initialized
Inflating...Done
Init MTS PORT to Serial Device
HW watchdog initialized to reset on 30 sec timeout, successfully.
Adding 2586 symbols for standalone.
rtc_ioctl(SET_RTC_ALARM): Rounding Secs val to next minute
WeekDay Alarm: Disabled at Sunday
Day Alarm: Enabled at 01
Hour Alarm: Enabled at 12
Minute Alarm: Enabled at 52
Current Time: 01Jul03 00:51:08
/tffs1 (upper FLASH) initialized OK
desired_gwy_id: 43
/tffs0/ANA_CAL.NVM unavailable
SER_boSerialInitOk
NVM_vdRestoreMsnFromNVM: fsize 24
Reading 1 MSN LL elements from NVM
MSN LL[0] Gwy 43 SCT: Msg 0 645710348 Gg 0 649627148 SCO: Msg 1 Gg 1 Rpt 1
J1708_retrieve_structs
dspInit: dsp_get_synthError_from_flash
Starting End-of-Line test.
Gateway = 1
DL channel = 271
Change channel number; recalculate Fletcher
SYNC: 0 0x65
SYNC: 1 0xa8
SYNC: 2 0xf9
SYNC: 3 0x01
SYNC: 4 0x10
SYNC: 5 0x0f
SYNC: 6 0x01
SYNC: 7 0x00
SYNC: 8 0x00
SYNC: 9 0x00
2 0x1d GWY INFO: 0x01 00 00 00 00 00 00 00
Set GWY ID to 1; recalculate Fletcher
DL_CHN_INFO:
UL_CHN_INFO:
EPH:
Sent DL Frame: channel 271, gateway 1, synthError 0
>>>>Init DIO for RELAYS<<<<
RELAY_NVM
Set D7 as output.
RTC expected
>>>Turning on sepic...
Best Regards,
Tom Daniels
Test Engineer
The Morey Corporation
100 Morey Drive
Woodridge, IL 60517
T: (630) 754-2256
F: (630) 754-2656
tdaniels@moreycorp.com
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".