AnsweredAssumed Answered

vrf Date: Tue, 9 Oct 2001 13:37:45 -0500

Question asked by rsb on Oct 9, 2001
Ross Bledsoe <RBLEDSOE@Coinco.com> wrote:
> Is there any way to use the Agilent Benchlink Data Logger software to
> capture, store and analyze data from instruments controlled by VEE
> applications automatically.
> Ross

If it can be done programatically then most likely you can do it from VEE.

I could easily be wrong but last I saw the Benchlink products
are standalone closed apps not capable of communications other
than to the specific instruments in question. No API, COMS or anything
else that would allow them to be controlled programatically. The
Benchlink manual I just looked at suggests that outputs can be
had by cut-and-paste from the displays- not a good indication.

If this is correct then the general answer is "no"

Can anyone confirm/deny this?

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes