<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=ISO-8859-1"><TITLE>Re: [vrf] VEE filenames...?</TITLE><META content="MSHTML 6.00.2800.1400" name=GENERATOR></HEAD><BODY><DIV><SPAN class=206542907-03052004><FONT face=Arial color=#0000ff size=2>Thanks, but it didn't help....</FONT></SPAN></DIV><BLOCKQUOTE dir=ltr style="MARGIN-RIGHT: 0px"> <DIV class=OutlookMessageHeader dir=ltr align=left><FONT face=Tahoma size=2>-----Original Message-----<BR><B>From:</B> Beliveau, Bruno [mailto:BrunoBeliveau@solectron.com]<BR><B>Sent:</B> den 29 april 2004 16:18<BR><B>To:</B> VRF<BR><B>Cc:</B> Alexander Poulikakos (KI/EAB)<BR><B>Subject:</B> [vrf] Re: VEE filenames...?<BR><BR></FONT></DIV> <P><FONT size=2>I am not sure it has a common cause, but we had a subject about 8.3 filenames a year ago. Here is a post from Georg Nied. Hope this will help.</FONT></P> <P><FONT size=2>-----Message d'origine-----</FONT> <BR><FONT size=2>De: Chule Walker [<A href="mailto:CWalker@rfmd.com">mailto:CWalker@rfmd.com</A>]</FONT> <BR><FONT size=2>Date: 29 avril 2004 09:27</FONT> </P> <P><FONT size=2>I've got this problem too on one of my machines but if I open Vee first and then File>Open or click the Open icon and browse to the file, the whole name appears. I remember uninstalling 6.01 before installing 6.2 so maybe that has something to do with it? 7.0 shows the full name but I have not installed it on the box with the problem. </FONT></P><BR> <P><FONT size=2>-----Original Message-----</FONT> <BR><FONT size=2>From: Alexander Poulikakos (KI/EAB) [<A href="mailto:alexander.poulikakos@ericsson.com">mailto:alexander.poulikakos@ericsson.com</A>]</FONT> <BR><FONT size=2>Sent: Wednesday, April 28, 2004 3:28 AM</FONT> </P> <P><FONT size=2>In the upper left corner of each VEE window there is the filename stated, for an example</FONT> <BR><FONT size=2>if the filename is "anyname.lib" the upper left corner says: "VEE Pro - anyname.lib".</FONT> </P> <P><FONT size=2>But when I have a filename that is longer than 8 characters, let's say: "utility_common.lib", the upper left corner it says: "VEE Pro - UTILIT~3.LIB".</FONT></P> <P><FONT size=2>I find this very annoying, especially when I have several files starting with the</FONT> <BR><FONT size=2>same 6 characters.</FONT> </P> <P><FONT size=2>I use VEE 6.03 on a Windows 2000 PC, my colleague who has the same kind of setup</FONT> <BR><FONT size=2>does NOT have this problem with filenames longer than 8 characters. </FONT></P> <P><FONT size=2>I assume it's some sort of settings that needs to be done in the OS, does anyone </FONT><BR><FONT size=2>knows where this can be set????</FONT> </P> <P><FONT size=2>Or can it have anything to do with if you install/uninstall different VEE versions and something in the registry gets korrupted?</FONT></P> <P><FONT face=Arial color=#000000 size=2></FONT> </P></BLOCKQUOTE>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
if the filename is "anyname.lib" the upper left corner says: "VEE Pro - anyname.lib".
But when I have a filename that is longer than 8 characters, let's say: "utility_common.lib",
the upper left corner it says: "VEE Pro - UTILIT~3.LIB". I find this very annoying, especially
when I have several files starting with the same 6 characters.
I use VEE 6.03 on a Windows 2000 PC, my colleague who has the same kind of setup
does NOT have this problem with filenames longer than 8 characters.
I assume it's some sort of settings that needs to be done in the OS, does anyone
knows where this can be set????
Or can it have anything to do with if you install/uninstall different VEE versions and something in the
registry gets korrupted?
/Alex
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".