AnsweredAssumed Answered

vrf USB Question

Question asked by aufenanger on May 18, 2004
At the moment I am looking to read some data from one USB-instrument without
USBTMC protocol. As I understand USB it should be very easy. Looking for all
connected instruments on USB and then read information from the oune you are
interested in.

Of course there should a solution with windows kernel dll's but there are a
lot of struct variables and so implementing in VEE ist a lot of work. So I
was looking for the Agilent VISA COM USB 1.0 Type Library. But I can find
nothing for help. No help file ans no help stings in function and object
browser.

Does anyone have documentation about this library?
Do anyone know if I can handle low level USB-handling with this library?
Or does anyone has some other dll's to handle low level-comands?

Very best regards
B. Aufenanger

------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen

Telefon          : (089) 613 984 91
Fax.               : (089) 613 981 23
Email             : mailto:Aufenanger@somatec.de
homepage     : http://www.somatec.com/
------------------------------------------------------------



---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes