<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 3.2//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META NAME="Generator" CONTENT="MS Exchange Server version 5.5.2654.45"><TITLE>Re: [vrf] VEE Error 957</TITLE></HEAD><BODY><P><FONT SIZE=2>Try to replace the junction with a new one. It may be a defective part (ie. corruption). It happenned to me a couple of times before...</FONT></P><P><FONT SIZE=2>-----Message d'origine-----</FONT><BR><FONT SIZE=2>De: Henrik.Hald@nokia.com [<A HREF="mailto:Henrik.Hald@nokia.com">mailto:Henrik.Hald@nokia.com</A>]</FONT><BR><FONT SIZE=2>Date: 2 juin 2004 08:51</FONT></P><P><FONT SIZE=2>I just had 2 Error 957 pointing to a simple junction (vee object) in a function.</FONT><BR><FONT SIZE=2>This function is not new, and therefore this can't be the fault.</FONT></P><P><FONT SIZE=2>I was using VEE version 6.01 the first time and 6.03 the second time.</FONT></P><P><FONT SIZE=2>Are there any ways to find the reason for this fault.</FONT></P>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
I just had 2 Error 957 pointing to a simple junction (vee object) in a function.
This function is not new, and therefore this can't be the fault.
I was using VEE version 6.01 the first time and 6.03 the second time.
Are there any ways to find the reason for this fault.
Venlig hilsen, Kind regards
Henrik Damborg Hald
Henrik.Hald@Nokia.com
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".