AnsweredAssumed Answered

vrf DAQ Interfaces

Question asked by rsb on Jul 28, 2004
"Amrik Sekhon" <amrik.sekhon@geeplus.biz> wrote:
> Hi All
>
> Slightly off the subject, but can anyone recommend a DAQ interface that
> works well with Vee.
>
> I currently use the instrunet Inet100. This is has been a good bit of kit.
>
> But for my next project i do not need as many I/O ports and was wondering if
> there are any cheaper alternatives.

I'm using a USB DAQ (PMD1208) from Mesurement Computing and so far
it works flawlessly from VEE. And is only a hundred bucks so very well
worth it. 16 bit digital IO, 2 channel DAC, 8 channel ADC , 32 bit counter,
powered by USB (no wall wart). They also have lots of other devices
which presumably will work as well.

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes