Hello,
I am a novice to VEE.
Could someone send me some example programs of about 4339B and 4294A for electronic measurement ?
-------------------------------------------------------------------------------------
15Һ˫,II--D4512466/D3532399 http://design.163.com/aocmonitor/index.html
آy˫+.n+}("&N.n+zwZnV隊[h:"XW(Ӣ칻 &ޱiZGj)m^jl+j z{r:,zwfz -bf)+-隊_ڂ)^ܢo!wv ^x%lzwZ,j 0l+j z{r
You could acquire in chunks, reading each piece into an array and dealing with it seperately.
We did a special version of intuilink for the deep memory 5462x scopes that would read large datasets and then examine them in pieces. The intent was bringing it into excel, but there is an active-x control and that should work.
Jay Nemeth-Johannes
Complete Test
720 SW 14th Street
Loveland, Colorado 80537
(970) 663-0006
www.completetest.com
> -----Original Message-----
> From: yuanliang pan [mailto:panyuanl@hotmail.com]
> Sent: Wednesday, July 28, 2004 3:58 AM
> To: VRF
> Subject: [vrf] how to get more than 2000 data points
>
> hi,
> for days i am troubled by this question. i am using the
> Agilent 54622D mixed oscilloscope. i use it to collect data.
> but i want to get more data than 2000. i set the scope work
> in the mode that the guide says so that the most data points
> can be got. the system reports that the most points can be
> 2M. but when i want to get data points more than 2004 the
> system will report error. the error is that it's end of data
> or no data.
> i don't know what happen? i set the scope as the guide,
> but no exact result. hehe. please help me. any reply will be welcome.
>
> _________________________________________________________________
> ä¸Žè ”æœºçš„æœ‹å ‹è¿›è¡Œäº¤æµ ï¼Œè¯·ä½¿ç”¨ MSN Messenger: http://messenger.msn.com/cn
>
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".