AnsweredAssumed Answered

86100D Trigger

Question asked by motoman89 on Mar 29, 2012
Latest reply on Apr 2, 2012 by motoman89
Hello!
We bought an oscilloscope. At the stage set-up revealed a problem with the time base. The oscilloscope detects the amplitude of the signal amplitude characteristics can be measured, but the signal is displayed as a continuous band on the screen. The oscilloscope does not react to changes in the time base. How to achieve the normal form of the displayed signal? It is necessary to collect a special scheme of measurements using a trigger connector on the front panel or not? Go to the oscilloscope module has also been raised 86107A precision timebase, but it is not yet installed in the base module. Is it possible to work without the oscilloscope module, or it is required? What should be the circuit connecting it?
Thank You!  

Outcomes